Back to top

 

 

All in one: One cable for all applications
Single-cable technology in servo drives: More than ten years of practical experience

Kollmorgen One-Cable LösungThe key theme of the discussions is essentially recognized; and the questions from neighboring disciplines, too. It goes something like: when does decentralized drive technology become worthwhile? When is it advisable to leave the frequency converters in the control cabinet? How high are the additional costs for shielded motor cables in centralized solutions when compared to higher device investment in robust "outdoor technology" with a high degree of protection? Machine and plant engineering now faces a similar question once again regarding the single-cable technology of servo motors. Kollmorgen brought this option onto the market ten years ago and now offers them as standard for synchronous servo motors of the AKM series. 

 

Also interesting for a colleague? Simply forward this email...

KOLLMORGEN Europe GmbH | Pempelfurtstr. 1 | D-40880 Ratingen | www.kollmorgen.com | 
+49.(0)2102.9394.0 | [email protected]

eNews subscribe | eNews unsubscribe | eNews - Archive | Privacy Statement

©2014 Kollmorgen. All rights reserved.