Back to top

Visit Kollmorgen at IPPE 2017 in Atlanta, Georgia

The International Production & Processing Expo is hailed as the largest annual trade show for poultry, meat and feed industries representing the entire chain of protein production and processing. The 2017 IPPE show will bring together over 1,200 exhibitors and 30,000 attendees in Atlanta from January 31 – February 2, 2017.

Make plans to stop by Kollmorgen booth B5176 to see how we help innovators in the Poultry and Food Processing industry make the world a safer place, or schedule a meeting in advance.

We look forward to seeing you at IPPE!

IPPE 2017 JAN. 31 - FEB. 2, 2017
Georgia World Congress Center
285 Andrew Young International Blvd NW
Atlanta, Georgia USA

Show Times
Tues., 10 A.M. - 5 P.M.
Wed., 9 A.M. - 5 P.M.
Thur., 9 A.M. - 5 P.M.