Back to top

Improving Sanitary Machine Design Webinar, May 12, 2016, 11:00 AM EDT

 

Join us Thursday, May 12th at 11:00 AM (EDT) for this informative webinar on "Improving Sanitary Machine Design"

Building or using machines that must withstand daily wash-downs?

Designing industrial equipment that produces thousands of pounds of food daily and is thoroughly washed to a microbiological level presents an engineering challenge. 

The proper selection of electrical components is critical to the success of the machine.

We will present material on the following topics: 

  • Review of electrical equipment in wash-down areas
  • Typical motor and gearbox failure modes
  • Durability issues: discussion of IP ratings - IP66, 66K, 67, and 69K
  • Ingress and effects of temperature and pressure on “sealed” systems
  • Why covers are NOT the answer
  • Results of food services survey conducted with 30 leading food safety and sanitation personnel
  • Financial justification: sanitary design & durability retrofit

This webinar will be recorded and made available to view on demand.

 

  

 

 

 


 

 

The webinar will last approximately 40 minutes followed by a Q & A session. 

Be sure to join us for this webinar on sanitary design May 12th at 11:00 AM EDT.