Skip to main content

Going Small - How Current Step Motor Technology Can Help You Reduce Machine Size >

As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…
Kollmorgen Blog

Getting the Best Performance from Encoders >

I often see some confusion in various customers’ minds regarding encoder performance with automation systems which have servo drives or variable frequency drives (VFD). Some customers feel that when they are providing best in class encoders,…

Applications Sizing - Part 1: Getting Started Sizing Servos >

Never sized a servo before? Well, we want to share with you some of the best practices we have found over the years. Over the next few months, we will continue this series with a variety of tidbits that will help you become more comfortable with the…

Eccentricity, Wobble, and How a Servo System Can Help >

By definition, Eccentricity is a measure of how much a roll deviates from being perfectly circular. Ideally, eccentricity should be zero, but in reality, it is never zero. Practically not a single roll is a perfect circle because it is produced using…
Kollmorgen Blog

4 Tips for Considering Your Servo Motors IP Rating in Your Application >

What should you consider when factoring IP Rating into your specification and what other environmental factors should be considered when specifying motion products? As a manufacturer of motion control products for a variety of markets, Kollmorgen…

Ethernet Networks Simplified >

Setting up an Ethernet network can be frustrating if you don't understand the basics. A network is just the communication connection between two or more devices. These devices can be computers, PLC's, servo drives, HMI's, sensors, cameras…anything…

Modbus TCP with AKD Compared to Fieldbuses >

Unlike fieldbus communications only being supported by particular models of the AKD servo drive, Modbus TCP communication is supported by all of the AKD models. Whether you have a simple "analog" drive, an indexing drive, or an AKD with BASIC…
Kollmorgen Blog

Get More for Your Money - Electric over Hydraulic in Oil and Gas >

A key driver for the current trends towards increasing use of electric motors in oil and gas applications is the ability of electrically driven systems to substantially improve system reliability, reduce downtime, and the limit the possibility of a…
Kollmorgen Blog

Feedback Choices - Hall Effect Device (Part III) >

Among the simplest and least expensive feedback devices are Hall-effect sensors.  These are digital on-off devices that detect the presence of magnetic fields.  Made of semiconductor material, they are rugged, can be operated at very high frequencies…
Kollmorgen Blog

Three Unconventional Uses for HMI's >

Most machine builders are familiar with modern touch screen HMI's. They have all but replaced older style toggle switch panels. It has also enabled machine builders give operators much more information on the process going on in a machine. HMI's can…

5 Tips for a Successful Servo Crossover >

There are a number of situations that call for crossing over and replacing an existing motor with a newer servo. These can include: product obsolescence, cost savings, lead time issues, or upgrading to newer technology. The specifics of each…
Kollmorgen Blog

Feedback - The Right Choice Makes All the Difference - Part II >

In our previous post of this series, we learned that the selection of a feedback device is critical for precise motion applications, and that where it's located is important as well. Today's post covers some additional information regarding the…
Kollmorgen Blog

Feedback - The Right Choice Makes All the Difference - Part I >

A critical element of any servo system is the feedback device - after all, that's what makes it a servo to begin with! How about a very simple example to start off with: I have a bow and arrow, a target 30 feet away, and I left my glasses at home. So…

Embedded Motion for Lightweight Robotics >

The utilization of robotics in manufacturing is currently a $5B industry and is projected to grow to a $20B industry (Source: A Roadmap for U.S. Robotics, From Internet To Robotics - 2013 Edition). A major contributor to the projected growth will…
Kollmorgen Blog

Evolution of Kollmorgen - Part 5 >

Quick recap form our last post: In 1948, the company called Inland was formed by an out-of-work immigrant whose net worth was approximately $4000. Six employees ran the facility in the basement and garage of the Unruh home. The company's first…