Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

Becoming a Kollmorgen partner means you get access to NDC Solutions – a complete automation kit in constant development.

Want to join the industry 4.0 revolution but don’t know where to start? Here is how AGVs can make a real difference at a modest investment.

Electro-Optical/Infrared (EO/IR) Systems are used to provide long distance visual and thermal imaging for a variety of applications. Often used in satellites, planes, and military applications, there are two main components found in EO/IR systems: sensors and the motion system. While both the sensors and motion systems need to be reliable in many environmental conditions, let’s take a look at the 5 Harshest Environments for EO/IR Motion Control Systems.

We cover the top 5 advantages of direct drive motors, where the system or motor is connected directly to the load, versus a conventional rotary system.

A collaborative robot (Cobot) is a robot intended to physically interact with humans in a shared workspace. This is in contrast with other robots, designed to operate autonomously. A "cobot" is a robot that works in tandem with a human worker. The assumption is that a cobot and a human can produce an end result better and faster than either could do working alone.
Huge demand for robots, cobots, AI and Industry 4.0 is driving innovation hubs across the globe.  Whether the focus is software, industrial robots, cobots, medical robots or something else - the best way to facilitate and attract talent is to huddle around academic centers and universities.  Thus is born a Robotics Cluster, which is a group of entities that – formally or informally – locate in close geographical proximity.

We’ve all seen the movies…the one where the ‘intelligent’ robots go off-piste and bring untold chaos to the human race.  It never really turns out rosy just as the end credit start to fall. However, regardless of Hollywood’s ‘predictions’, no matter where I go or where I look (as part of my role in Kollmorgen’s Aerospace & Defence team) I am constantly tripping over a growing exposure to robotics and Intelligent robots in the Defence sector; air, land, sea and subsea.

If you experience some unintended motion or unexplained drive faults in your motion system, there are several possible causes. For example, motion setup through the drive, a poorly designed program within the control, and motor or feedback commutation phasing 180 degrees out can all cause unintended motion. For this review, we’re going to look at issues created by the contribution of poorly chosen and installed motor cables.

Throughout the Iron Man series, Tony repeatedly tells the articulated cobot that he’s doing it wrong, he even goes so far to place a dunce cap on its head and put it in the corner. And this brings me to an important aspect of a cobot: teachability.

Who you are defines how you think of robotics and automation.  Software experts and IT may think of internet bots.  They might also think about the new, emerging field of Robotics Process Automation (RPA), which is software that can do mundane and administrative computer tasks.  RPA reduces repetitive tasks such as checking, verifying and transferring data.  Manufacturing facilities will think about physical robots or cobots that are also deployed to handle repetitive tasks such as loading and unloading a CNC machine or installing a computer cover.  They can also be used to automate dangerous tasks such as lifting, welding or removing paint.