Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

Never sized a servo before? Well, we want to share with you some of the best practices we have found over the years. Over the next few months, we will continue this series with a variety of tidbits that will help you become more comfortable with the job of sizing a servo. In this post, we’ll start with the basics of good preparation.

So everyone’s heard the phrase “think outside the box.”

And at Kollmorgen we do that. But the reality is we have to think about inside the box. It’s our job to protect inside the box. Our OEMs need us to be ever conscious of inside the box so that the box works and is dependable. But OEMs also look outside the box - does it fit, is it smaller, what’s the advantage?

By definition, Eccentricity is a measure of how much a roll deviates from being perfectly circular. Ideally, eccentricity should be zero, but in reality, it is never zero. Practically not a single roll is a perfect circle because it is produced using a machine which itself is prone to some machining errors (since it is product of some other machine and so on).

What should you consider when factoring IP Rating into your specification and what other environmental factors should be considered when specifying motion products?

As a manufacturer of motion control products for a variety of markets, Kollmorgen Application and Sales engineers get involved in specifying products into all kinds of environments. Often these environments can be wet and thus an IP (International Protection) rating needs to be considered as a part of the specification of our product.

Setting up an Ethernet network can be frustrating if you don't understand the basics. A network is just the communication connection between two or more devices. These devices can be computers, PLC's, servo drives, HMI's, sensors, cameras…anything that supports Ethernet communication.
Unlike fieldbus communications only being supported by particular models of the AKD servo drive, Modbus TCP communication is supported by all of the AKD models. Whether you have a simple "analog" drive, an indexing drive, or an AKD with BASIC programming, you have the capability of using Modbus communication. It is a simple, easy to use, standard communication protocol that can be used in a PC, PLC, or HMI to talk to any AKD drive.

A key driver for the current trends towards increasing use of electric motors in oil and gas applications is the ability of electrically driven systems to substantially improve system reliability, reduce downtime, and the limit the possibility of a leaked fluid discharge into the environment. Designers of oil and gas equipment are looking for the smallest, lightest, simplest solution with the least impact on the environment. While the best solution will be different for every application, it’s clear that the trend in the industry is favoring electric motors.

Today’s blog is part of a Throw Back Thursday post – about an article I wrote for SubNotes magazine back in 1988. At the time we had completed a number of submersible motor applications for some very unique and tough environments. Applications with interesting names like Alvin, Jason Jr, or Robin – the first, a manned research vehicle at the time operated by Woodshole Oceanographic Institute, the other two, remotely operated submersibles used to explore the wreck of the Titanic, among other adventures.

This blog was originally posted back on June 18, 2012 - I wanted to update this with some new activities regarding our work with Universities since that date...

There has been a long standing cooperation between Industry and Academics throughout the recent centuries. Just look at the companies that pop up near Universities - like the Route 128 corridor near MIT, or Silicon Valley's influence by Stanford, UCB and UCSF. Every major research university houses a "technology park" filled with start-ups incubating their new ideas and inventions. But it's not just the entrepreneurs that latch on to collaboration with academics. Established firms also find it beneficial to work with universities on various projects of interest, especially where an emerging industry may be getting ready to take off.

Among the simplest and least expensive feedback devices are Hall-effect sensors.  These are digital on-off devices that detect the presence of magnetic fields.  Made of semiconductor material, they are rugged, can be operated at very high frequencies (equating to tens of thousands of motor rpm), and are commonly used to provide six-step commutation of brushless motors.