Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

So, you’re beginning to size a new servo motor and drive for an application. How do you go about doing this? Sizing tools can be highly beneficial for achieving optimized products. However, one needs to pay attention to the warnings and information provided in sizing systems.

We cover the top 5 advantages of direct drive motors, where the system or motor is connected directly to the load, versus a conventional rotary system.

A collaborative robot (Cobot) is a robot intended to physically interact with humans in a shared workspace. This is in contrast with other robots, designed to operate autonomously. A "cobot" is a robot that works in tandem with a human worker. The assumption is that a cobot and a human can produce an end result better and faster than either could do working alone.

If you experience some unintended motion or unexplained drive faults in your motion system, there are several possible causes. For example, motion setup through the drive, a poorly designed program within the control, and motor or feedback commutation phasing 180 degrees out can all cause unintended motion. For this review, we’re going to look at issues created by the contribution of poorly chosen and installed motor cables.

Frameless, or “servo motor kits”, open up numerous possibilities in designing motion elements for your machine related to performance.  A frameless motor consists of rotor and stator components which are built into a machine assembly to transmit torque to a load.  Many applications which take advantage of a frameless motor are direct driven, which eliminates bandwidth robbing compliance.  Effectively, this means you have eliminated torsional losses and any wind-up or spring losses. 

A collaborative robot (or Cobot) is a robot that is made to work with or interact with human co-workers. For most of us normal folks, the most well-known example is Tony Stark’s robotic arm. (For those reading who are wondering why I don’t refer to the arm as JARVIS, it’s because JARVIS is the AI and controls other things but not the robotic arm.) Tony has bit of an unhealthy relationship with the robotic arm, he insults it, puts it in a dunce cap, puts it in time out, or threatens to dismantle it. At which point the robotic arm usually hangs his robotic limb downward into sadness. But, the robotic arm is there to do work for Tony in his basement. He may have a large house, but he doesn’t want a 10-foot-tall robot behind a fence. He wants an assistant, a co-worker of sorts that can help build his Iron Man suits.

Until the start of the new millennium, it was customary practice to purchase drives, motors, and cables from different suppliers. Nowadays, connection cables are no longer considered to be an accessory but a product in their own right that requires a level of competency similar to that of any other product. Only the company that designed the motors and drives is in a position to make the appropriate choices to offer its customers a high quality and flexible connection that can be tailored to their application requirements.

Robots and automated machines and vehicles form an integral part of our everyday lives and are not just found in the industrial sector: precise control of motion is indispensable. The combination of the two areas of technology – motion (servo drives) and movement (AGVs) – allows KOLLMORGEN to play a leading role in “Motion in Movement – 4.0 Ready” solutions, and to offer its own customers complete and integrated systems, ready for Industry 4.0.

These 3 characteristics are crucial when sizing a motor for any application from military to industrial and beyond. In this day and age where everything seems to be getting smaller and more compact, we all want our toys to take up less space, but we don’t want to sacrifice any performance. Let’s use cars as an example. When someone is shopping for a sports car, they may be looking for things like high speed, quick acceleration, low center of gravity, small body, etc. These are all reasonable things to look for in a sports car. However, if someone was to say, “I need a two-door sports car with a top speed of 160mph, but I also need it to tow my 10,000 lb trailer”, we might have a problem. This is the same principle when we’re talking about motors. Just like cars, generally smaller motors have much higher speeds than larger motors. However, the large motors are the ones towing that 10,000 lb trailer, or in our case, exerting the most torque.

Search the web for frameless or kit motors and you will find many offerings to choose from.  When looking at the motor specifications, there are many important parameters to consider such as rated speed, rated current, peak current, etc.  What do all these things mean and why is it important to understand how the values are being presented?