Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

We are excited to introduce the launch of a brand new product selection tool – Kollmorgen Stepper Optimizer. Optimizer provides multiple ways for you to discover what Kollmorgen stepper motor works best in your application. Comprised in the tool are Kollmorgen’s most highly recommended stepper series. This includes our newest stepper product, the PMX Series, as well as our  popular Powermax and POWERPAC product families.
Horsepower (hp) is a measure of power, which can be further described as the rate at which work is performed.  There are slightly different definitions for its conversion to the unit watts depending on the mechanism being described: mechanical, electric, boiler, metric, etc..   Our focus here will be on servo motor systems.

For many, “Made in Italy” is synonymous with Italian ceramic tiles, but did you know most tiles have been handled by “someone” other than Italian workers?

Read the exciting story on how Volvo introduced AGVs in their production. Even if 1973 seems 100 years ago, the technology is more relevant than ever.

Europe's second largest dairy company, Arla Foods, has been using AGVs in their facilities since 2009. Read more to see how Arla Foods ensures everyone "gets milk."

Most of us have been there at one point or another…..wishing we had a backup copy of something. Whether it’s contacts on a cell phone or a program file in a motion controller, data is important and valuable.

The next generation of industries is facing new challenges. What role can Automated Guided Vehicles play?

Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications.  In order to achieve the highest level of performance, the linear motor system must be commissioned properly.  This blog post addresses key areas to consider when setting up and commissioning a linear motor system.  It is always important to refer to the installation and set -up instructions provided by the manufacturer.

Markus Johansson was appointed General Manager of Kollmorgen Automation AB on October 12, 2015.

Question: I need to operate a servo motor in a vacuum, what are some considerations? 

Answer: In a word?  Outgassing.  You might think that proper motor sizing is a big issue, it always is, however if you can't conform to the other process requirements, there is no point to attempting to size the motor.  The biggest issue for any given motor selection to be run in a given vacuum for a specific process is the outgassing requirement, or rather, the avoidance of materials that would affect the process being performed and/or the life of the motor.