Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

There are several considerations when selecting a servo motor for a specific application, such as the required speed, torque or force, motion profile, available physical envelope, and environmental factors. This means that the chosen motor solution must produce the load torque and speed requirements, fit in the available space, and perform as required under the subjected environmental conditions of the application.

Bode plots have existed since the 1930’s when Hendrik Bode devised a way to display gain and phase-shift plots in the frequency domain. Today, to produce a detailed frequency response plot that reveals the unique fingerprint of a servo mechanism in the frequency domain is as simple as pressing a computer key. This paper discusses five key items in a Bode plot and what they reveal about the machine.

A servo motor is an electromechanical device that produces torque and velocity based on the supplied current and voltage. A servo motor works as part of a closed loop system providing torque and velocity as commanded from a servo controller utilizing a feedback device to close the loop. The feedback device supplies information such as current, velocity, or position to the servo controller, which adjusts the motor action depending on the commanded parameters.

A collaborative robot (Cobot) is a robot intended to physically interact with humans in a shared workspace. This is in contrast with other robots, designed to operate autonomously. A "cobot" is a robot that works in tandem with a human worker. The assumption is that a cobot and a human can produce an end result better and faster than either could do working alone.
Huge demand for robots, cobots, AI and Industry 4.0 is driving innovation hubs across the globe.  Whether the focus is software, industrial robots, cobots, medical robots or something else - the best way to facilitate and attract talent is to huddle around academic centers and universities.  Thus is born a Robotics Cluster, which is a group of entities that – formally or informally – locate in close geographical proximity.

The human vs. robot topic in workplaces has been in the spotlight for quite a while. Look at the comments under the YouTube video where Google introduced its AI (Artificial Intelligence) assistant that could call restaurants and salons to make appointments - there is widespread concern from the audience over the risk of human workers being replaced by AI-equipped machines. But on the other hand, even Elon Musk admitted in a Tweet that “humans are underrated” at Tesla, where “excessive automation was a mistake”. Inspired by such arguments, I keep pondering over one question: what is the role of robotization, or automation in a broader sense, in today’s employment?

A few years ago I watched the DARPA challenge. If you’re not familiar with the challenge, the idea was to build a robot that could drive a car, climb a ladder, turn a handle, use a drill and various other activities.  In the challenge each robot was given an hour to complete the tasks.  It was a slow process. I had two reasons to watch, one, Kollmorgen has some frameless motors in the Carnegie Mellon robot and two, I’m a Virginia Tech graduate and they also provided a robot.
A collaborative robot (or Cobot) is a robot that is made to work with or interact with human co-workers. For most of us normal folks, the most well-known example is Tony Stark’s robotic arm. (For those reading who are wondering why I don’t refer to the arm as JARVIS, it’s because JARVIS is the AI and controls other things but not the robotic arm.) Tony has bit of an unhealthy relationship with the robotic arm, he insults it, puts it in a dunce cap, puts it in time out, or threatens to dismantle it. At which point the robotic arm usually hangs his robotic limb downward into sadness. But, the robotic arm is there to do work for Tony in his basement. He may have a large house, but he doesn’t want a 10-foot-tall robot behind a fence. He wants an assistant, a co-worker of sorts that can help build his Iron Man suits.

Usually, in discussion about these terms, we tie in the word actuator – so more precisely, what is the difference between a linear actuator vs a rotary actuator?

Linear actuators, in essence, move something along a straight line, usually back and forth.  Rotary actuators, on the other hand will turn something a number of degrees in a circle – it might be a limited number or an infinite number.

So, linear actuator – back and forth, Rotary actuator - round and round

Over Christmas my family and I traveled to Cape Canaveral, Florida to visit the Kennedy Space Center. Since the trip (and even before) my house has been a buzz about rockets, astronauts, count downs, stages, boosters, and did I mention rockets? Naturally, I was one of the 3 million people to watch the launch of the Falcon Heavy live. And over the last few days, there have been several things that I have found myself reflecting on – and it isn’t nostalgia for the space race – its excitement.

Pages

Blog Taxonomy Helper

Aerospace & Defense
Applications
Automated Guided Vehicles
Business
Embedded Motion
Engineering
Fieldbus
Food Regulations
General
History
Installation Tips
Interconnectivity
Medical
Oil and Gas
Packaging
Robotics
Technology
University Partnerships
Subscribe to Blog in Motion