Back to top

Welcome to Kollmorgen's Blog in Motion.  We have been adding information and knowledge to the great web based world for many years - through white papers, technical documents, and even webinars.  Kollmorgen enjoys sharing our knowledge with you, as well as identifying other motion related tidbits through our Twitter, Facebook, LinkedIn and YouTube feeds.  Our newest source is Blog in Motion, covering a wide range of topics, as well as some interesting contributing authors with lots of Motion experience.  If Motion Matters to you, stop by, follow, like, and sign up so you can stay tuned for what Kollmorgen has in store for you!

How do I calculate a motor’s continuous torque when it is operating in an environment above its rated temperature? Since the motor’s continuous torque (Tc) is rated in a 40°C ambient, how can I estimate the motor’s continuous torque during my worst-case ambient temperature of 55°C?  

Installing and integrating AGVs involves project organization, driveway design and system connection. Here is what you need to think about.

Installing AGVs in your plant is about change management. How do you convince your people that automation is the right way to go?

More than ever, we are shopping on the net, putting pressure on companies to keep up with their intralogistics.

Learn your AGVs the smartest driveway with teach functionality.

Local or specialized AGV supplier? How to find the right one.

Collaborative robots are designed to work safely with and next to their human counterparts.  A subset of collaborative robotics has innovative safety techniques that completely eliminate the need for a safety barrier between the human and the robot.  This enables a wide range of applications to deploy and benefit from this collaborative robot technology.

Buying AGVs? Read this checklist to avoid the pitfalls.

We are excited to introduce the launch of a brand new product selection tool – Kollmorgen Stepper Optimizer. Optimizer provides multiple ways for you to discover what Kollmorgen stepper motor works best in your application. Comprised in the tool are Kollmorgen’s most highly recommended stepper series. This includes our newest stepper product, the PMX Series, as well as our  popular Powermax and POWERPAC product families.
Horsepower (hp) is a measure of power, which can be further described as the rate at which work is performed.  There are slightly different definitions for its conversion to the unit watts depending on the mechanism being described: mechanical, electric, boiler, metric, etc..   Our focus here will be on servo motor systems.