Back to top
A few years ago I watched the DARPA challenge. If you’re not familiar with the challenge, the idea was to build a robot that could drive a car, climb a ladder, turn a handle, use a drill and various other activities.  In the challenge each robot was given an hour to complete the tasks.  It was a slow process. I had two reasons to watch, one, Kollmorgen has some frameless motors in the Carnegie Mellon robot and two, I’m a Virginia Tech graduate and they also provided a robot.

This blog was originally posted back on June 18, 2012 - I wanted to update this with some new activities regarding our work with Universities since that date...

There has been a long standing cooperation between Industry and Academics throughout the recent centuries. Just look at the companies that pop up near Universities - like the Route 128 corridor near MIT, or Silicon Valley's influence by Stanford, UCB and UCSF. Every major research university houses a "technology park" filled with start-ups incubating their new ideas and inventions. But it's not just the entrepreneurs that latch on to collaboration with academics. Established firms also find it beneficial to work with universities on various projects of interest, especially where an emerging industry may be getting ready to take off.

In July of last year I posted a blog about the CHIMP robotic platform. CHIMP stands for CMU Highly Intelligent Platform. It was one of 16 entries under the DARPA (Defense Advanced Research Agency Projects) sponsored Robotics Challenge program with the goal of developing robotic technologies that can be used in harsh environments such as man-made or natural disasters in lieu of humans. The robots will be required to open doors, turn valves, connect hoses, use hand tools to cut through panels, drive a vehicle, clear debris, and climb a ladder.

The tragic earthquake and subsequent Tsunami that devastated the Fukushima Prefecture in Japan just over 2 years ago points to a great potential use of evolving robotics technology.  The Defense Advanced Research Projects Agency (DARPA) has created a competition among industry called the Robotics Challenge.  The challenge is to develop robotics technology that can eventually replace the need for humans to don those highly fashionable and comfortable HAZMAT suits as they go into very dangerous environments to keep a bad situation from growing worse.