Back to top
When a load is driven directly by the motor, the conversation around reflected inertia goes out the window. The belief is that direct driven loads do not, by their nature, have a reflected inertia. Some folks are even confident enough to say that the ratio of the load inertia to the motor inertia does not need to be taken into account when direct driving the load as long as you have enough torque and speed. I have never had enough confidence to make such a statement.

Sabotage!

21 Aug 2013
, by
“You clown’s don’t have a chance in hell! You can’t stump me!” I ranted to our team after successfully solving another challenge. The competition heated up. Just days before I had set up a linear slide system with a servo motor and drive, and challenged each of my teammates to ‘break’ the system and challenge me to fix it. The ‘winner’ who stumps me gets lunch, on me. Essentially they were contract saboteurs

There are challenges for a servo motor's protection against overheating by the manufacturer, machine designer/OEM, and user, because there is no thermal device that can protect a motor against a fast transient event.  For just as there is a time lag between the final steady-state temp rise of a coil of wire with a given current going through it, there is a time lag for the thermal device to achieve its trip resistance once that trip/application temperature has been presented to the thermal device.

There is a lot of energy [pun intended, sorry] going into the design of next generation, high temperature, Down-Hole motor technology at Kollmorgen. The existing motor technology available in the marketplace has basically been the same since the inception of brushless motor for Down-Hole use by Kollmorgen back in 1986. Sure, the magnet technology has improved; giving us higher performance Samarium Cobalt magnets that hold up great in the high temperature extremes of the Down-Hole environment, but the basic insulation systems and motor materials haven't changed much.

Electric motors are used in machines and processes all around us.  You can find them in factories, automobiles, airplanes, robots and even your favorite DVD vending machine.  Regardless of the application, managing heat dissipation is a common theme. Electric motors are often selected based upon a particular work or load requirement.  One consideration of this selection process is managing heat dissipation.  Although electric motor design is constantly improving, all generate heat through losses and inefficiencies.  This needs to be evaluated when selecting the proper motor for your needs.

While all of this work by Fredrick Kollmorgen was going on another immigrant, named Hugo Unruh, was growing up in Germany. About the same age as Frederick’s son Otto, Hugo faced the harsh conditions in post WWI Germany with its rampant inflation and struggling economy. His family encouraged him to emigrate to the United States so he could realize his dreams.

Hugo was partially educated in Germany, but finished high school and two years of college while in the US. To help get through school, Hugo worked as a repairman at an X-Ray company.

Prior to leaving Europe, Fredrick became the proud father of a baby boy – Ernest Otto. This would be the first of three children, the other girls (Hildegard and Dorthea). From various records, I can only piece together a few bits of information regarding the early 1900’s. It appears Frederick’s wife (Agnes Hunt), an English woman, whom he married in Italy, traveled back and forth to the United States from England, bringing the children over at certain times. Otto was born in 1901 and came to the US in 1907, two years after Fredrick immigrated. Hildegard, was born in 1903 and followed to the US in 1910. Finally, Otto’s youngest sister, Dorthea, was born in 1914 in Italy –right in the midst of World War I.

Over the next few months, we will be publishing a blog series about how Kollmorgen evolved from its humble beginnings to today. Follow us on this journey and learn about the visionaries that built the foundation of our company.

Turn back time – to the 1900’s, the turn of the century, the industrial revolution in full force. A young man who was skilled in optics left his homeland of Germany to work under the auspices of optics pioneer, Karl Reichert in Vienna. Frederick Kollmorgen decided to bring his skills to America, passing through London with a brief stint with Ross, Ltd. Kollmorgen settled in New York, providing optic skills for Keuffel & Esser, who manufactured drafting and surveying instrumentation.

Noise, and I'm not talking about that terrible band you heard at the summer fest last year, but electromagnetic interference (EMI) noise. There are 8 key steps to consider when trying to eliminate EMI noise issues. If you follow these guidelines, you are much less likely to have problems with electrical noise in your application.

There really isn't anything to fear when utilizing high performance frameless servo motors in your machine design. Many engineers get concerned about "air gaps" and "concentricity" when discussing frameless servo motors - but there is little to be afraid of! In applications where an embedded motor design makes sense, the application shaft that the frameless motor will be mounted on will already be machined to tolerances well within the range required for robust servo driven performance. Concentricity, run out, and axial play all must be considered in the machine mechanism itself and will typically be well in range for the KBM motor family. With the use of high energy magnet materials, the need for an ultra-tight air gap is out the window!