KOLLMORGEN equips its S700 servo controllers with single-cable connection technology

Kollmorgen S700 Servo Drive Single cable

Ratingen/October 2017 - The benefits of connecting drives using just one cable are obvious in machinery and plant construction: they include faster installation, space savings, reduced inertia, and lower costs to name a few. Following very positive experiences with the AKD and AKD-N servo drives, KOLLMORGEN is now also equipping the talented all-rounder S700 with its pioneering single-cable connection technology.

The KOLLMORGEN servo controllers from the SERVOSTAR series S700 are primarily designed to fulfill particularly complex drive tasks – with safety technology up to and including SIL3. The devices can be programmed freely with macro support in IEC 61131-3 based language. The S700’s features also include cogging compensation for excellent radial run-out characteristics.

KOLLMORGEN is connecting the in-house developed digital resolver SFD or high-resolution Hiperface DSL encoder with one standard motor cable through the single-cable connection technology now available for the S700 controllers. The result is a cost-efficient and slender installation solution which reduces costs while also helping to increase machine performance - starting from space gains to more speed when positioning, as less cable needs to be moved at the same time.

Image caption 1.1
Designed for sophisticated tasks and now also including slender single-cable connection technology: the S700 from KOLLMORGEN combines multi-functionality with maximum levels of freedom from programming to wiring.

Image caption 1.2
Designed for sophisticated tasks and now also including slender single-cable connection technology: the S700 from KOLLMORGEN combines multi-functionality with maximum levels of freedom from programming to wiring.
 

 

Kollmorgen Press Kit

 

ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact think@kollmorgen.com or visit our website www.kollmorgen.com/uk