Skip to main content

Kollmorgen Support Network

Herzlich willkommen beim Kollmorgen Support Network (früher KDN). Hier finden Sie Unterlagen zum Herunterladen, können Fragen stellen und einer Community beitreten

 

 

Site Statistics:
872
Contributions
Registered Users
1518
Articles
2743
Downloads

Latest Support Articles

KAS v4.02 Software is now available!KAS v4.02 Software is now available!
Prashanth Morishetty
AKD2G System Configuration with Kollmorgen DDL Linear MotorsThis document shows the wiring requirements for connecting the DDL linear motors to the AKD servo drive. It also describes the setup procedure for configuring the AKD2G drive in the Workbench software.
toddevans01
AKD2G DS402 and Manufacturer Specific Torque and Current Setpoint and FeedbackFor AKD1G ECAT users the objects 2071h and 2077h do not exist. See the following app note for equivalents with the AKD2G ECAT drive.
toddevans01
S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero…
Kollmorgen Support
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos.
Rodrigo Gallo Rodrigo Gallo

Latest Community Topics

profiles creation
jay thomas
Homed reference point retained during power down?
njandroep
S400 Drive program COM1 fail
MolnaarBence
Add new AKDn on existing AKDC
bcharpentier
Linear Motor Service mode
Tamim

Online-Ressourcen

Sie haben nicht das gefunden, was Sie brauchen? Unten finden Sie zusätzliche Kundendienst-Optionen wie ausführliche Unterlagen für KAS und AKD, Links zu unserem Schulungsbereich und Dokumente von Anbietern.