Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

Joe Parks's picture
Joe Parks
1 week 4 days ago
Watch a video which shows how to add multiple languages inside one project in the Kollmorgen Visualization Builder (KVB) software. Using a built-in action, the user can change all the strings in an HMI project at once from one language to another. This is helpful as only a single project has to be maintained, no matter where in the world it might be shipped.
Dan.Wolke@Kollmorgen.com's picture
1 week 6 days ago

Hypertherm is a CNC for laser/plasma cutting machines.  We have received some reports on issues with setting up AKD drives being used with this machine. Following are some tips.

toddevans01's picture
toddevans01
2 weeks 5 days ago

This is part 2 of a two part series. This application note will demonstrate establishing Modbus TCP communications between a Kollmorgen Visualization Builder ( AKI ) project and the variables in a running program in the AKD BASIC drive. Reading and Writing are demonstrated much in the same fashion as Part 1 but using KVB instead of Modbus Poll.

toddevans01's picture
toddevans01
2 weeks 6 days ago
This application note serves as a quick start with simple example using a Modbus Master simulator software called Modbus Poll to read/write over Modbus TCP to/from the AKD BASIC program ( variables ). This is part 1 of a two part series. Part 2 will demonstrate similar methods but using the Kollmorgen Visualization Builder software for our AKI operator panel product line.