Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

dusty.schafer's picture
dusty.schafer
2 weeks 4 days ago

New Features

  • AKD2G Drive Integration:
    • Single and Multi-Axis drive variants
    • Position and Time-based Capture
    • Feedbacks #2-5
    • Simplified User Units and Synchronized with WorkBench
    • Support for AKDG2 firmware v2-02
    • Remaining feature(s) not yet available: Backup/Restore
  • Map EtherCAT feedback to PLCopen Digitizing Axis
  • Multiple IDE Instances
  • IDE Ease-of-Use Enhancements:
Leonardo Souza's picture
Leonardo Souza
2 weeks 6 days ago

Em aplicações rotativas com encoders absolutos multivoltas é possível que o controlador perca a contagem do número de voltas. Se a máquina usa um redutor com redução de acoplamento não binária (Ex. 3:1), o periodo da máquina não é um divisor inteiro se comparado com o periodo do encoder, possibilitando que posição de feedback não seja a mesma após desligar e ligar a máquina.

Leonardo Souza's picture
Leonardo Souza
3 weeks 42 min ago

On a rotary application with absolute multi-turn feedback, it's possible to run over the feedback unwind. If the machine has a non-binary gear ration (e.g. 3:1), its period is not an integer divisor of the encoder period, allowing the position to not be the same after a power cycle. In other words, it may be shifted by the fraction of the ratio.

jcoleman02's picture
jcoleman02
3 weeks 22 hours ago

Touch Probe Overview