Skip to main content
press_release | Significant Lead Time Reduction |
|
minute read

WOOD DALE, IL – Thomson, A Danaher Motion Company, has significantly reduced lead times for some of its most popular Thomson slides. Lead times for Thomson 2DA, 2CA, 2BA, IB Series, IC Series, ID Series and IV Series linear guides have been reduced to just 2 days. Lead times for Thomson 2DB, 2EB, MS, 2HB, 2HE, 2RB AND 2RE driven systems have been reduced to just 4 days. The new lead times are effective for orders of 5 pieces or fewer. Lead times for higher quantities will remain 10-20 days, depending on the particular series of Thomson slide ordered.
“The lead time reduction is intended to get high quality Thomson slides quickly into the hands of machine builders who are prototyping a new machine or redesigning an existing one,” says Jim Marek, Business Unit Manager, Thomson Linear Systems. “We receive a large number of requests from OEMs who are looking to improve machine performance, and reduced lead times in limited quantities enables them to put Thomson quality to the test within the real time constraints these engineers are facing.”

About Thomson
With more than 60 years of motion control innovation and quality, Thomson is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case™ Shafting, ground and rolled Ball Screws, Linear Actuators, Gearheads, Clutches, Brakes, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945, and has set the standard ever since with an unsurpassed set of mechanical motion control solutions serving global commercial and aerospace & defense markets. Thomson, a Danaher Motion company, has facilities in North America, Europe and Asia with over 2000 distributor locations around the world.

Das Außergewöhnliche entwickeln

Wir bei Kollmorgen glauben an die Kraft von Antriebstechnik und Automatisierung bei der Erschaffung einer besseren Welt.

Erfahren Sie Mehr