Personal Mobility

Danaher Motion image

Kollmorgen leads the market in Personal Mobility based on vast application experience, innovation, and scope in motion controls technology.


As a strategic platform of Kollmorgen we have the financial strength to invest in advanced technologies and we continuously work towards providing our customers a competitive advantage in their respective markets. Kollmorgen development engineers continuously work on transferring existing knowledge and experience to new customer applications. Our deep knowledge of lift truck, driverless control systems, and electromechanical actuators is being applied in numerous other electric vehicle markets.

  • Power Chairs

  • Wheel Chairs

  • Scooters

  • E-bikes

  • Mobility Scooter

 

Danaher Motion image

PMAC Motors


Kollmorgen engineers put their pride in developing a motor to fit each customers needs. For example, Kollmorgen developed a PMAC motor for the Segway- a motor with breakthrough torque density and built-in sinusoidal feedback. The Segway motor features dual windings that when connected to a dual drive, allows for complete redundancy. This makes for virtually two motors in one mechanical package and should one fail, the Segway still functions. Kollmorgen Engineers are currently fine tuning the qualities of a permanent magnet AC Motor(PMAC) solution for lift truck applications. The PMAC motor is approximately 10-15 percent more efficient than an induction motor, enabling smaller size and/or batteries and/or longer work shifts.