Company
Kollmorgen - 运动控制专家。
Kollmorgen公司结合了超过30个行业领先的品牌(例如,Kollmorgen、Thomson、Dover、 Pacific Scientific、Portescap、Neff、Seidel和Bautz),建立了专注于客户的运动控制制造与服务公司,称为Kollmorgen。在Kollmorgen品牌下我们可提供功能强大的集成运动控制技术。我们是年销售超过10亿美元的全球运动控制领先者,汇集几十年应用经验和技术创新,致力于帮助客户更好、更快的制造机器。
Kollmorgen定义了高标准的质量、创新和技术。我们能够在控制成本的同时提高机器性能和可靠性。我们的全球制造足迹、快速定制以及原型制作能力,驱动着快速订货至交货时间。无与伦比的应用经验和设计专家经验使用户能够更快速地调试机器。
在当今竞争激烈的运动控制市场上,作为一个值得客户信赖的合作伙伴,Kollmorgen全球的6,100名员工凭借超过60年应用经验,加上2000多家经销商,将竭尽全力助您事业成功。Kollmorgen可服务于半导线、航天和国防、电力车辆系统、包装、印刷、医疗以及机器人等各种行业。用户需要时,通过遍布全球的服务和技术支持基础设施、现场服务工程师和技术支持团队,我们可提供一种无比深度和广度的运动控制产品解决方案。
Motion is at our core
We consistently maintain the highest standards of quality, innovation and technology. We help you build in exceptional motion performance, reliability and longevity, while considering cost and time-to-market challenges.
Broadest Range in the Industry
Our breadth of products allows for a range of solutions—standard, modified or custom. You can depend on our integrated, optimized components and hit the ground running in any application with ease.
Helping You to Build Differentiated Equipment
With Kollmorgen, you’re getting great value and strength. We leverage a team of more than 1,800 employees, and over 60 years of application experience applied to selecting the optimum motion components for your machine.
Exceptional Motion Control Partner
Our range of best-in-class components is unparalleled. Our application expertise and our rapid customization and prototyping capabilities help you build differentiated equipment and get it to market faster.
Kollmorgen 基本数据
- 丹纳赫集团旗下业务平台,年销售额超10亿美元
- 产品设计中心遍及全球
- 地区分布
- 北美50%
- 欧洲40%
- 其它地区10%
- 拥有6,100名员工
- 全球工程、运营及支持网络
- 超过2,000 个分销地点
- 生产设施占地210万平方英尺
- 纽约证券交易中心(NYSE)交易代码:DHR