|
A DANAHER MOTION COMPANY |
APRIL 2009
|
| |
GET CONNECTED: Is Inferior Cabling Compromising
the Performance of Your Machine?
|
Engineers designing servo and stepper systems tend to focus on the obvious: the motor, controller, amplifier, and sensors. Signal and power cables, though no less important than the components they connect, are often overlooked until the project's end, or worse, handed off to an electrician without proper training. The result: lower-than-expected accuracy, frequent failures, low immunity from electromagnetic interference (EMI), and adverse effects on neighboring equipment.
Find out more>>.
|
 |
SIMPLIFY: Standardize on a Single Servomotor Family
with Global Features-Set
|
|
As internal engineering resources continue to be eliminated or outsourced, designers are being asked do more and in less time. While the aggressive pursuit of new global markets increases the potential for revenue growth, machines must now meet a number of varying design specifications and requirements for use in the global marketplace. As profit margins become thinner, a machine must be less complicated, more economical to manufacture and be supported anywhere in the world. What is needed, of course, is simplicity to make the design process easier.
Kollmorgen AKM brushless servomotors are designed with those challenges in mind. They are engineered to satisfy global application needs by delivering unprecedented choice and flexibility from a single product platform. With 26,000 standard models available, AKM high performance servomotors offer a wide range of mounting, connectivity, speed, feedback and other options, as well as a variety of windings designed to support standard global voltages. AKM motors can be paired with a Kollmorgen
S200, S300,
S600 & MMC Smart Drive high performance servo drive for a fully optimized servo system.
Find Out More>>
|
 |
WORK SMART: Maximize your Machine Performance
with Multi-Axes High Performance Motion Control System
|
Available in 2 to 64 axis stand-alone and 1 to 16 axis drive resident versions, the stand-alone Digital MMC is a high performance, full-featured multi-axis motion controller that communicates to servo amplifiers using a high-speed Ethernet-based digital motion control network. Real-time information from the drive is available to the application program via the digital link.
Find out more>>. |
 |
|
WHAT'S NEW: Multi-Axis Motion Control Systems Now Available
|
Kollmorgen is pleased to announce the release of DS4 and DS6 Linear Tables used in multi-axis Cartesian motion control systems for precision positioning, high-speed automation, and robotics.
No need to source and integrate individual components. The fully-integrated system provides a turn-key solution that drastically reduces system integration time otherwise required by the customer.
To create 2D/3D models of the tables, please visit our online modeling tool.
Contact us today your most challenging multi-axis applications! Call 540-633-3400 or visit us online. |
 |
|
Keep an Eye Out...
|
For the highly anticipated Advanced Kollmorgen Drive™ (AKD) coming this Fall. As advanced, scalable, Ethernet-based servo drives, the AKD family of drives will deliver cutting-edge technology and performance with one of the most compact footprints in the industry.
Feature-rich and versatile, the AKD drive provide a solution for nearly any application, from basic torque and velocity applications to indexing, while setting the standard for power density and performance.
Do more with less. Outperform the competition with the most versatile drives on the market. Contact us today to find out more. |
 |
| Motion 101 - SERVO/Step Product Introduction & Application Sizing |
| Controls | Apr 21 - 23, 2009 | Radford, VA |
| AM 101 - Applied Mechanics - LMS Components, Product Line & Applications |
| Linear Motion Systems | Apr 28 - 30, 2009 | Radford, VA |
| AM 201 - Advanced Mechanics |
| Linear Motion Systems | May 12 - 14, 2009 | Radford, VA |
| MEI 301: Develop Advanced Control Algorithms with Mechaware™
|
| Controls | Apr 20 - 24, 2009 | Sunnyvale, CA |
| MEI 101: MEI Boot Camp |
| Controls | May 4 - 8, 2009 | Santa Barbara, CA |
| MEI 102: Troubleshooting Techniques for MEI Motion Controllers |
| Controls | May 18, 2009 | Santa Barbara, CA |
|
|
Contact Us
|
|
Kollmorgen
203A West Rock Road
Radford, VA 24141 US
|
Phone: 1-540-633-3400
Fax: 1-540-639-4162
Email: [email protected]
|
About Kollmorgen e-News Kollmorgen e-News is a regular motion control engineering and innovation update providing news through significant educational articles and product information from Kollmorgen and other expert sources.
|
|