Success Stories

 

KOLLMORGEN Alesa DentaCombi 160

Alesa - Grinding Machine - Cutting edge: The shark teeth

Saw blade manufacturer Alesa develops its own grinding machine with Washdown servo motors from KOLLMORGEN with single-cable connection technology.
More
   
Kollmorgen KBD Coilhandling

KDB - Coil Packaging System - Hard as steel: 2.5 tons with a high degree of efficiency

Direct drive with braking modules from KOLLMORGEN provides noticeable energy savings in coil handling.
More
   
Comau Kollmorgen – a flexible solution for the smart factory

Comau – AGV – Comau’s first AGV: a flexible solution for the smart factory

The Turin-based giant chooses the motion control specialist as its AGV solution provider
More
   
KOLLMORGEN Functional Safety Technology

Kollmorgen - Safety - The risk with vertical axes

Controlling and monitoring brakes are part of functional safety technology at KOLLMORGEN
More
   
KOLLMORGEN MEQuadrat AKD-C power supply unit thumbnail

MEQuadrat - Rotary Indexing Table - Providing orientation for materials

Swiss company MEquadrat AG builds test systems with decentralized servo technology from KOLLMORGEN
More
   
New potential with a separate labeler

VH Vertical Packaging - New potential with a separate labeler

Why VH Vertical Packaging is developing its own solutions and why servo drives with 48 volts from KOLLMORGEN are the perfect match
More
   
buhler kollmorgen success story

Buehler - Pre-Ferment Application - A perfect solution in Bakery Automation

For the pre-ferment, Bühler has developed a solution - JetMix - Better hygiene thanks to KOLLMORGEN’s stainless steel servo motor
More
   
Kollmorgen-SwissCan Thumb

Swiss Can Machinery - Filling Application - Anything but trivial: filling milk powder into cans

Scaled technology and functioning interfaces are essential for Swiss Can Machinery / Hygienic drives from KOLLMORGEN
More
   
Packman 200 & Kollmorgen

Opteq - Mobile Robots - Self-driving systems for internal material flow

DC servomotors in KOLLMORGEN’s AKM series with 48 volt winding for autonomous vehicles
More
   
Flexibility and Innovation for Top Printing Quality

OMET - Flexographic Printing Machine - Flexibility and Innovation for Top Printing Quality

AKD-N decentralized drives and CDDR motors by Kollmorgen are the core of the innovative OMET Xflex X5, a printing solution with the best returns on investment in terms of market result of narrow web printing of labels and flexible packaging.
More
   
Kollmorgen_Servo Technique_Centralized_Decentralized_Machine

Kollmorgen - Centralized or Decentralized?

Which architecture type delivers the best technical and commercial advantages?
More
   
Excellent Mailing service thumbnail

C.M.C. srl - Printing and Packaging Machine - An Excellent Press Mailing System

Decentralizing the system to reduce space and materials
More  
   
Kollmorgen Todema Coltal Machine

Todema - Printing Machine - For Automated Decoration

CDDR Direct Drives and AKD PDMM Motion Controllers for accurate lacquering of screw caps
More  
   
Kollmorgen Mezit AKD and AKD PDMM Servo Drives

Mezit Technology - Industrial Digital Printing Machine Manufactured For the First Time in Turkey

Digital Printing Accelerated With Contributions From Kollmorgen
More  
   
Kollmorgen - Zinser 4125 Application involving drilling and cutting unit

Zinser - All-Purpose Flame-Cutting Machine - Cuts through like a knife through butter

Metalworking: Zinser opts for Kollmorgen servo technology in its CNC cutting center
More  
   
High impact customized solutions

MEquadrat - High impact customized solutions

Interconnected engineering service increases productivity and creates tangible added value
More  
   
Nort Thumbnail Double Innovation

Nort Makina - Double Innovation In Paper Bag Machine

Automatic System offers 30% Increased Performance in Production and Mold-Switching Process
More  
   
Kollmorgen CA TecoDrive

tecodrive - Material Feed Application - Magnetic field instead of feed rollers

tecodrive is developing a revolutionary process for material feed applications with the help of servo drives from Kollmorgen
More  
   
AKD-N Thumbnail - 2016 language story  

Kollmorgen - Decentralized servo technology without language barriers

KOLLMORGEN develops a multi-language interface for Profinet, Ethernet/IP, EtherCAT & Co.
More  
   
Kollmorgen Tisse Hybrid Machine

Tisse - Plastic Injection Machine - Maximum Speed and Energy Efficiency with Hybrid Design

First in Turkey in the field of Plastic Injections, Tisse and Kollmorgen have together developed an electric-hydraulic Hybrid Machine.
More
   
Kollmorgen Salvagnini Application

Salvagnini - Panel Bending Machines - Distributed servo technology bends panels into better shape

Salvagnini simplifies the design of its machines using drive solutions from Kollmorgen
More
   
Kollmorgen_Bottero_small

Bottero - Glass Processing Plant - Grinding with half of the axes

At Bottero Group, KOLLMORGEN’s AKD series drives perform multiple functions
More
   
Kollmorgen_Kuka

KUKA - Compact Robots - Even higher power density

Kuka and Kollmorgen co-engineer optimised motors for compact robots
More
   
Kollmorgen IMAPG

IMA-PG - Packaging Machine - 450 Blisters per Minute

PLC, motion control, drive as one unit: A complete solution for PG Express
More
   
Kollmorgen Proteck Rack System

Protek - Cutting-edge laser machining

Latest machine-generation with cost-efficient mechanical transmission designs
More
   
Kollmorgen_Tenco5_RX-9011_EN

Tecno5 - Glass printing

Direct Drive Technology Prints a Better Picture
More
   
Kollmorgen_Lollipop_MotorGear_EN

Lafer - Complete Motion Solution For Packaging

Schleck enjoy the aromatic double
More
   
Kollmorgen_schleuter_labelmachine_EN

Schleuter - Labeling Machine - 360 degree labeling with direct drive

Joint development: Motion control solution with integrated labeling controller
More
 
Kollmorgen_Einkabellösung_Success_Story

Kollmorgen - All in one: One cable for all applications

Single-cable technology in servo drives: More than ten years of practical experience
More
 
Kollmorgen_Multivac_Packaging Machine

Multivac - Packaging Machine - Electrically Deep Drawn Packages: Faster Sealing Without Pneumatic

Quieter, more efficient and improved controllability: MULTIVAC uses Kollmorgen’s servo competency
More
 
Kollmorgen_Univeral_Robots_Robots

Universal Robots - Articulated-Arm Robots - Better motors for more options - Kollmorgen drives the lightweight helpers of Universal Robots

A large part of the power density of the six-axis articulated robots comes from specially adapted KBM motors from Kollmorgen. Universal Robots was able to embed the motors directly into the articulation axes without need for additional housings.
More
 
Kollmorgen_Prinovis_Success Story

Prinovis - Rotogravure Printing Press - How Prinovis Reduced Scrap, Increased Throughp ut and Ensured Future Flexibility with Dynamic Motion Solution from Kollmorgen

In search of new controllers for register control of a rotogravure printing press, Prinovis Itzehoe GmbH implemented a new motion control solution from Kollmorgen that produced important, measurable results.
More
 
Kollmorgen Jakob_Success Story

Jakob Graphic Services - Jumbo Roll Collator - Kollmorgen Automation Suite™ delivers dynamic performance to maximize productivity of fully automated modular paper processing machine

The RC-500J jumbo roll collator, manufactured by the Germanbased Jakob Graphic Services GmbH, is raising the bar when it comes to processing a wide variety of printed continuous paper products.
More
 
Kollmorgen Pole Position_Success Story

Ball Racing Developments - Racing Simulators - Kollmorgen parts put BRD in pole position

Formula One racing teams demand the highest performance from every single component, which is why motion system specialist, Ball Racing Developments Ltd, uses high quality parts supplied by Kollmorgen.
More