Hannover Messe 2017: KOLLMORGEN will exhibit the AKD2G servo amplifier and PCMM motion controller at the joint ETG stand.

The second generation of servo drives speak EtherCAT

Ratingen, April 2017 – A real-time Ethernet system for motion and safety: KOLLMORGEN uses EtherCAT as the system bus for the second generation of AKD2G servo amplifier. High-performance communication with EtherCAT also plays a vital role for the new PCMM motion controller. Both devices will be exhibited by KOLLMORGEN at the Hannover Messe from 24 to 28 April 2017 at the ETG user organization stand in Hall 9, Stand D18.

Machinery and plant manufacturers have a real advantage when safety technology communication is incorporated into the machine’s existing real-time communications. With this in mind, the second generation of KOLLMORGEN AKD2G servo amplifier uses FSoE - the EtherCAT safety protocol - for safe communication. As safety and motion both run over the same cable, the need for additional secure wiring together with EA safety modules to control the safe motion functions has been eliminated. The AKD2G is particularly impressive in this regard: With safe brake control (SBC) and the integrated safe brake test (SBT), KOLLMORGEN provides an important safety function, for, as an example, the vertical axes on the controller side.

Picture 1
The new AKD2G generation of servo amplifiers from KOLLMORGEN uses EtherCAT as the system bus.

Picture 2
High-performance communication with EtherCAT also plays a vital role for the new PCMM motion controller.

Kollmorgen Press Kit

 

ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact think@kollmorgen.com or visit our website www.kollmorgen.in