sps ipc drives: KOLLMORGEN once again awards "Partner of the Year"

Ratingen 25. January 2016 - The two European partner prizes awarded by KOLLMORGEN form a North-South axis in 2015. By awarding it to Delta Elektronik from Taastrup, the prize lands at the gates of the Danish capital, Copenhagen. Significantly further South, IBD GmbH from Munich has been serving customers in high-tech areas for more than twenty years. Both of the organizations recognized at sps ipc drives are KOLLMORGEN "Silver Partners".

Delta Elektronik holds the silver status awarded by the specialists in servo drive technology and motion control from Ratingen since 2011. Recognizing the Danish organization with the award acknowledges its commitment to serve the Scandinavian machine building industry with individually tailored system solutions. Delta Elektronik is also one of the established experts in equipping installations with decentralized servo technology based on the KOLLMORGEN AKD-N series as well as tasks in hygiene areas – achieved using fully decentralized Motion Control solutions from the AKD-N servo drive and AKMH stainless-steel servo motors.

IBD GmbH from the Bavarian state capital has been serving customers in the high-tech areas of general machine building, laser technology, plant construction, and automobile industry for more than twenty years. Success here comes as a result of everything from the needs-based selection of the drive solution, to engineering services, and to integration in the plant. Smaller switch cabinets, less cabling, slimmer design: The organization is one of the first KOLLMORGEN partners to have triggered an innovation boost in the field of machine building with the decentralized AKD-N servo drives.

Kollmorgen Press Kit  

Image 1
The Delta Elektronik Team, Jesper Rissbøll, Thomas Sommer and Christian Bahn, are happy about their “Partner of the Year 2015” award.

Image 2
Managing Director Franz Hangl accepted the "Partner of the Year" award on behalf of IBD GmbH from CEO Dan St. Martin and Managing Director for Germany, Jan Treede.

About Kollmorgen
Kollmorgen is a leading provider of integrated automation and drive systems along with corresponding components for machine builders all over the world. With more than 70 years of Motion Control Design and application experience and profound knowledge of constructing standard and special solutions, Kollmorgen supplies solutions time and again that stand out in terms of performance, quality, reliability, and ease of use. As a result customers can achieve a market advantage which is beyond question. For further information please contact think@kollmorgen.com or visit our website www.kollmorgen.com/hi-in