Kollmorgen Medical Robotics

Surgical Automation

Minimally invasive surgery is the way of the future. Improving on the technologies of conventional laparoscopy and arthroscopy, surgical robots are providing surgeons with greater visibility, dexterity, precision and comfort than ever before. 

 

Today’s surgical robots decrease operative trauma, improve patient outcomes and shorten lengths of stay in prostate, cardiac, gynecological and many other types of surgery. And their growth potential is unlimited as new surgical applications are developed and as hospitals add new capabilities to better compete for patients.

The Most Demanding Motion Environment: The Operating Room

Precise control of multi-axis motion, with coordination across all surgical controls, cameras and instruments, is the key to surgical robotics. This requires the highest-quality servo motors, drives and motion controllers working together seamlessly over a high-bandwidth motion network. But it’s not just about quality. It takes a complete motion solution, integrating components that are designed to work together within the most demanding application requirements and space constraints. These are Kollmorgen’s signature strengths.

The Right Tools and Skills

Kollmorgen offers the industry’s most advanced servo motors in configurations and torque ranges to meet virtually any specification. Our compact frameless and cartridge motors provide direct rotary motion for the stiffest, most exact motion in the smallest possible space – without the need for complicated and bulky transmission components. We also provide the integrated drives, controls, development tools and expertise needed to bring an optimized motion solution from the drawing board to the operating room.

A Tireless Assistant

Quality should always be the number-one concern in the healthcare setting. Repair and maintenance time is time that could be spent treating patients, instead of rescheduling their appointments. Through the Fortive Business System, our kaizen-based quality assurance and continuous improvement programs have made Kollmorgen the recognized leader in high-end motion. And with our global supply, engineering and support network, the components and expertise to keep robots performing are always near at hand. So the robot is always on the job.

KBM Medium

KBM Series Motors

KBM™ Series Motors eliminate the need for gears and transmission components to deliver the most precise motion possible.

More about KBM Series Motors >>
TBM Series Medium Image

TBM Series Frameless

The Kollmorgen TBM (Torquer Brushless Motor) Series direct drive frameless motor is designed to be directly embedded in your machine, using the machine’s own bearings to support the rotor.

More about TBM Series Frameless >>
AKM Medium png

AKM Servo Motors

AKM™ Servo Motors offer more than a million standard configurations, plus co-engineered modifications to meet any need.

More about AKM Servo Motors >>
AKMH 265x265 Image

Stainless Steel AKMH Series

The new AKMH Series is built to withstand the most rigorous of washdown regimens. The combination of the AKMH’s IP69K construction and corrosion resistant materials, make for a servo motor that will last the life of your machine.

More about Stainless Steel AKMH Series >>
Housed DDR Medium

Housed D & DH

Housed DDR servo motors offer high torque density, precise performance and zero maintenance in an easily installed servo solution.

More about Housed D & DH >>
CDDR image medium

Cartridge DDR Motors

Kollmorgen Cartridge DDR® motors combine the space-saving and performance advantages of a frameless motor with the ease of installation of a full-frame motor.

More about Cartridge DDR Motors >>
IC Series Ironcore (DDL) medium image

Direct Drive Linear

Direct Drive Linear Motor technology brings compactness, stiffness and simplicity to linear motion.

More about Direct Drive Linear >>
AKM-Gearmotor Medium

Gearheads

Our gearheads incorporate TRUE Planetary™ gearing for high torque capacity, smooth operation and minimal maintenance. So you can count on optimum performance, whether you need a general-purpose gearhead, an ultra-precise model, a washdown or food-grade version, or a complete gearmotor.

More about Gearheads >>
US Production