Image-Guided Intervention
Interventional
angiography, core needle biopsy, LITT and other procedures that require
placement of invasive tools within the human body depend on accurate
visualization. X-ray, CT, MRI and other imaging tools used in these procedures
need to move with absolute steadiness and precision to provide the view
required at any given moment, without blurriness or motion-related artifacts.
High-Quality
Images for High-Quality Care
Perfect
motion means that doctors can perform delicate procedures quicker, with greater
precision and less operative trauma. That’s good not just for the patient, but
also for the clinician and the healthcare facility. Because these imaging
machines need to be compact and infinitely adaptable, they require motion
solutions that work together in confined spaces to provide total stiffness,
smoothness and control. Motion matters because the image – and the patient –
matters.
Complete
Solutions – Optimal Performance
Kollmorgen
makes perfect motion happen with the industry’s most compact and precise
servomotors. Our frameless and cartridge servomotors mount directly to the load
to eliminate compliant transmission components and minimize space requirements.
We offer servomotors in configurations and torque ranges to meet virtually any
high-performance specification without the time, expense and risk of a
commissioning a custom motor. And we offer complete solutions that integrate
drives, controls, development tools and co-engineering services, enabling the
most advanced scanner designs to achieve full performance.
A Scanner
Clinicians Can Trust
Reliability
is crucial during a medical emergency. Even when routine work is disrupted by a
maintenance issue or mechanical problem, the clinic or hospital can pay a big
price in unproductive hours, rescheduled patients and general disruption.
Kollmorgen’s kaizen-based approach to quality assurance and improvement places
us at the top of the motion industry for precision and reliability. And our
global supply, engineering and support services ensure reliable access to the
products and expertise needed to keep scanners performing better, longer.

AKD™ Servo Drives provide industry-leading power density, performance and precision in one of the most compact footprints available.
More about AKD Servo Drives >>
AKM™ servomotors offer more than a million standard configurations, plus co-engineered modifications to meet any need.
More about AKM Servomotors >>
Kollmorgen Cartridge DDR® motors combine the space-saving and performance advantages of a frameless motor with the ease of installation of a full-frame motor.
More about Cartridge DDR Motors >>