Missles & Guided Munitions
In precision strike warfare, accurate targeting is of paramount importance. From the earliest inertial systems through “line-of-sight” systems such as laser or IR guidance, targeting efficiency has continuously improved while putting fewer air crews at risk. The addition of GPS, for example in JDAM systems, has enabled even more precise targeting in all weather conditions while allowing crews to “fire and forget” as they take evasive action and proceed to the next target.
Exact control in extreme conditions
Even with the most precise targeting inputs, the accuracy of any guidance system depends on the rapid and reliable positioning of fins and other control surfaces. Control actuation systems must be capable of delivering precise motion, at high torque, in instant response to constantly changing inputs. And because a single failure can mean a total loss of control, these systems need to survive extremes of temperature, altitude, dust, moisture, vibration and shock.
Top performance, dependable supply
Despite these strict performance and durability requirements, control actuation systems need to be as light as possible to maximize flying range and responsiveness. They also need to be affordable and reliably available in the configurations and quantities needed to upgrade existing weapons and replenish arsenals as the weapons are used. Kollmorgen servomotors have been incorporated widely in the defense industry’s most advanced control actuation systems to meet all these demanding requirements.
Co-engineering for a stronger defense
Kollmorgen offers proven co-engineering capabilities, working with a variety of defense contractors to design and build highly integrated control subsystems. Nearly 20 years ago, we helped pioneer the JDAM kits that convert “free-fall” bombs into smart munitions. Today, we’re helping make next-generation weapons systems even more accurate, at greater range, no matter how adverse the conditions. Expertise, performance, delivery and price—Kollmorgen delivers all the elements needed to coordinate a precision strike.

Direct Drive Servomotors
Kollmorgen direct drive brushless servomotors are available in housed, cartridge and frameless models for the lightest weight and most compact integration. We can modify or custom-build motors to meet virtually any torque specification, space constraint and operational requirement.
More about Direct Drive Servomotors >>
Global Manufacturing and Support
Kollmorgen operates engineering, manufacturing and support facilities in every major region of the world. Our co-engineering teams ensure an exact fit for your application, and our global supply chain ensures reliable supply in the quantities you need, on time and on budget.
More about Global Manufacturing and Support >>