Press Releases - 2015

  • 12/16/2015

    Learn How to Reduce Risk of Food Recall and Boost Efficiency Through Hygienic Machine Design with Kollmorgen at IPPE 2016

    Kollmorgen will exhibit its industry-leading motion solutions for food and beverage manufacturers in booth B8016 of the International Production & Processing Expo (IPPE), January 26 – 28, 2016, at the Georgia World Congress Center in Atlanta. Throughout the show Kollmorgen will demonstrate its AKMH Hygienic Servo Motor and enhancements, including the vented connector option, which allows the motor to equalize pressure through the connector assembly.

    Read More
  • 8/10/2015

    Kollmorgen Demos Next Generation of PMX™ Series Stepper Motors and AKMH™ Hygienic Servo Motors at PACK EXPO 2015

    RADFORD, VA - August 10, 2015 - Kollmorgen will exhibit its industry-leading motion solutions  at PACK EXPO , September 28 - 30, 2015, at the Las Vegas Convention Center. Visitors to booth C-1741  can expect to see the company's latest PMX TM  Series Stepper Motors and AKMH TM  Hygienic Servo Motors, and learn how they deliver improved productivity and higher throughput as a result of reduced maintenance and longer component life. Kollmorgen will also show off new enhancements to servo boxing - Vegas-themed servo boxing with a twist!

    Read More
  • 7/21/2015

    Kollmorgen Releases Next Generation of Stepper Motors: Broader Range of Frame Sizes, High-Performance Motors

    RADFORD, VA - July 21, 2015 - Kollmorgen is pleased to introduce the next generation of stepper motors, the PMX series, adding smaller 08, 11, and 14 frame sizes to the traditional 17, 23 and 34 frame size offering. Thanks to a wider range of sizes and options, OEMs now have added flexibility to meet multiple performance and application needs from a single motion source. Each frame size is built with high quality construction which translates to reliability in the field and long service life.

    Read More
  • 4/16/2015

    Kollmorgen Gives Away Segway® i2 SE Personal Transporter at PACK EXPO 2014

    RADFORD, VA - April 16, 2015 - Kollmorgen announces that Mark Rogenski is the winner of the company's Segway ® i2 SE Personal Transporter (PT) giveaway at PACK EXPO 2014. The Segway i2 SE PT is powered by a Kollmorgen electric motor that delivers 40% more torque per unit of volume than comparably-sized motors. It is a self-balancing, electric-powered transportation device designed for efficiency and maneuverability over a variety of terrain - from inside the warehouse to more challenging outdoor environments. Sleek and versatile, the Segway i2 SE PT is built with an anodized, height-adjustable LeanSteer™ frame and includes a wireless InfoKey™.

    Read More
  • 4/1/2015

    Kollmorgen and ReliantHeart Team Up To Produce Energy Efficient, Wireless LVAD

    RADFORD, VA - April 1, 2015 - ReliantHeart, Inc.,an innovative supplier of advanced mechanical circulatory assist technologies, and Kollmorgen,a leading provider of motion systems and components, announced a partnership to produce an energy efficient motor stator designed to cut the power consumption of the HeartAssist5® Left Ventricular Assist Device (LVAD) by 50%.

    Read More
  • 1/7/2015

    Learn How to Increase Food Safety and Efficiency Through Hygienic Design of Machinery Components with Kollmorgen at IPPE 2015

    RADFORD, VA – January 7, 2015 – Kollmorgen will exhibit its industry-leading motion solutions for food and beverage manufacturers in booth B7861 of the International Production & Processing Expo (IPPE), January 27 – 29, 2015, at the Georgia World Congress Center in Atlanta. Visitors to the Kollmorgen booth can expect live demos that illustrate how the company’s AKMH Hygienic Servo motors deliver improved productivity and higher throughput as a result of reduced maintenance and longer component life.

    Read More
US Production