RADFORD, VA – April 20, 2011 – Kollmorgen’s Power Generation System has been named a 2011 Golden Mousetrap best new product finalist by the editors of Design News magazine.  The Power Generation System is a complete, robust power platform that can be optimized to meet virtually any heavy-duty vehicle’s energy requirements, with the flexibility to fit in applications where space is at a premium.  The system readily accommodates vehicle upgrades and retrofits without any need to replace the generator, wiring or drive electronics.  It is being used by the United States Army to deliver 30kW of on board vehicle power (OBVP) generation at 28VDC to their Fuel-Efficient Ground Vehicle Demonstrator (FED).

 

“The products highlighted in this year's Golden Mousetrap winners and finalists clearly demonstrate both cutting-edge design ideas and the practical evolution of technologies for systems and product design engineers.  Design News congratulates all the engineers and their companies who have been recognized with the Golden Mousetrap Award, and we are grateful for their contribution to this year's competition,” says David Greenfield, Editorial Director, Design News.

 

For more than two decades, the Design News Awards Program has recognized engineering innovation and creativity in product design.  This year, Golden Mousetrap awards were given in four major categories: Electronics & Test, Automation & Control, Design Tools: Hardware & Software, and Materials & Assembly.  Managing Editor Jennifer Campbell gathered a record number of entries, distributing them to Design News beat editors for judging. 

 
“With the Power Generation System, Kollmorgen can provide the power that OEM’s need at the voltage they want.  And unlike vendors who supply just high or low voltage systems, we are uniquely positioned to serve as a one-stop shop for heavy-duty hybrid vehicle OEM’s who have a wide variety of power needs within a single vehicle, and/or across vehicle platforms,” says Mike Crowe, Director, Product & Technology Planning, Vehicle Systems, Kollmorgen.  “As application demands evolve, commercial and military hybrid vehicle OEMs adjust their designs and need to find the optimum voltage to deliver the desired power, so working with a single supplier who can deliver low or high voltage solutions, or anything in between, is a huge advantage.”

 

Heavy-duty hybrid vehicle designers have neither the time nor the capital to take unnecessary risk on unproven technology.  The Kollmorgen Power Generation System is rooted in mature technology backed by more than 60 years of motion control and power generation expertise that is now being implemented in heavy-duty hybrid vehicle applications to supply heavy power demands within a small space.  Consisting of a Kollmorgen permanent magnet AC generator, generator controller, software and cables, the system has the flexibility to support any heavy-duty hybrid vehicle power need at low or high voltage, AC, DC or both. 

 

The generator provides twice the power density within the same space as a traditional alternator, can be air- or liquid-cooled, and can be mounted in belt-driven, PTO or inline configurations.  The generator controller is rooted in a product platform with more than one million units delivered since 1996.  The controller features a robust, modular architecture that is engineered to withstand the most demanding commercial and military environments, and that facilitates easy expansion as vehicle needs evolve.  Cables are shielded and optimized for heavy-duty vehicle applications.  They consume minimal space and weight, while delivering maximum performance and reliability even in temperatures up to 260°C.

 

“Conventional hybrid motors and alternators simply aren’t engineered to satisfy the strenuous power demands of heavy vehicles.  These vehicles require a high-kilowatt system that’s small and adaptable enough to fit the vehicle without requiring a lengthy and costly redesign, and that supply the AC and DC voltages the vehicle requires,” explains Crowe.  “The Kollmorgen Power Generation System is just such a system.  Rather than imposing limitations, it opens up a world of new possibilities that makes vehicles more efficient, enables faster upgrades and provides the power needed to get the job done.”

 
Electrical power is an ideal technology partner to the internal combustion engines in heavy-duty hybrid vehicle.  It offers outstanding torque, efficiency, economy and cleanliness to supplement fossil fuels on urban buses, agricultural vehicles, military vehicles and other heavy-duty hybrids.  Electric power is also an increasingly significant tool for powering auxiliary equipment, from trash compactors on garbage trucks to armored doors on defense vehicles.

ABOUT KOLLMORGEN
Kollmorgen is a leading provider of power generation and motion systems for OEMs around the globe.  Through world-class engineering knowledge, industry-leading quality and deep expertise in linking and integrating standard and custom products. Kollmorgen delivers breakthrough solutions that are unmatched in performance, reliability and ease-of-use, giving vehicle and machine builders an irrefutable marketplace advantage.  For more information visit www.kollmorgen.com, email support@kollmorgen.com or call 1-540-633-3660.