- 12/4/2009
Compact Electric Cylinders are Competitively Priced to Displace Pneumatics and Hydraulics, with Improved Performance, in Small Thrust Applications
Radford, VA - Kollmorgen introduces EC1 Electric Cylinders. The EC1 is a cost effective, high-performance linear positioning alternative to pneumatic and hydraulic systems in applications requiring continuous thrust of ≤150 lb. (660N).
Read More - 11/3/2009
Increase Order Picking Productivity up to 100% and Decrease Operational Costs up to 40% with Pick-n-Go® from Kollmorgen
Radford, VA - Kollmorgen introduces Pick-n-Go® - a highly flexible order picking system that streamlines any order fulfillment process for exponentially higher picking productivity and significantly reduced operating expenses.
Read More - 6/3/2009
New Motion Programming Script (MPS) Enables Simple Programming Environment for Electrical and Mechanical Engineers without C-Code Expertise
Santa Barbara, CA - Kollmorgen introduces the new Motion Programming Script (MPS) — an easy-to-use, network-enabled implementation of a BASIC-like programming language with commands added specifically for motion control.
Read More - 5/31/2009
Kollmorgen and Sky-Trax Enter Into Strategic Alliance and Supply Agreement
RADFORD, VA – Kollmorgen and Sky-Trax Inc., announced today a five year partnership that provides Kollmorgen with the exclusive rights to distribute navigation and localization products from Sky-Trax. Distribution of the Sky-Trax products will be under the Kollmorgen brand.
Read More - 1/23/2009
New Kollmorgen LS5 Navigator Tough Laser Navigation Sensor for Rough Conditions
Radford, VA - Kollmorgen introduces its fifth generation of laser navigation sensors - LS5 Navigator. This is the first sensor designed not only for indoor use but also for outdoor environments and cold storage, paving the way for new applications with automated guided vehicles.
Read More