Skip to main content
Success Story | 2 minute read

A COMPARISON OF DECENTRALIZED AND CENTRALIZED SERVO TECHNOLOGY

Centralized or Decentralized?

Which architecture type delivers the best technical and commercial advantages?

 Kollmorgen_Servo Technique_Centralized_Decentralized_Machine

Decentralizing servo technology can bring machine and plant construction savings during installation. Two additional advantages include reduced cabinet heat loads and more straight forward drive architecture. The question arises however, which technology is better, an integrated motor/drive solution or a detached motor and drive?

So often in life the answer to a question is neither A or B, but instead C. This is true for the discussion of decentralized versus centralized servo technology in determining the best system. What architecture is best from a commercial and technical standpoint for a particular application? Instead of A or B, the answer C comes about through mixed architectures, a coexistence of both types. In this case the two approaches can be easily combined when the drives have a large number of common features. As such, standardization of these platforms is the best approach.

The centralized architecture

In contrast to horizontal conveying where decentralized servo drives are a common sight, centrally located servo drives are still dominate the market for highly dynamic and precise motion control. Servo drives along with other control components, sometimes with a full blown IPC, reside together in a control cabinet protected from the outside world. Connection to the motors is in a star shaped structure, each having control and power cables. Because heat loss is centrally generated, effective air conditioning is needed in the cabinet.

Kollmorgen_Servo Technique_Centralized_Decentralized_AKD-NThe decentralized alternative

Decentralized servo technology follows the basic principal of shifting the individual motor control from the central control cabinet to be closely located to the process This architecture makes necessary a robust design providing a high degree of environmental protection. The advantage lies particularly in terms of motor cabling. Two other advantages are improved EMC-behavior and the widespread distribution of heat loss, reducing the cost or need for a centralized cabinet climate control system.

Trends in machine building industry

Especially with packaging machinery and machines for the food and beverage industry, the trend is away from meter long cabinet walls but instead installing small, highly self-protected units within the machine frame. The progressive trend is toward modularization of production facilities making necessary the distribution or combination of functions. This statement is reinforced by the fact that production equipment consist of a main process and ancillary tasks. The latter are a variety of compatible modules – for example conveyor systems, sorters and handling units. This provides a path for easy expansion of the machine. Against this backdrop, practical experience shows that a decentralized structure is advantageous, especially with spatially distributed single axes. In contrast, machine modules for synchronized axis physically close together and centrally located drives in a cabinet are generally considered the preferred structure.

Kollmorgen_Servo Technique_Centralized_Decentralized_Servo-drive-architectureMonetary savings in installation and mounting

The savings potential of decentralized technology can be clearly shown based on a real metal forming machine having eight axes. The first axis of which is located 5 meters away from the control cabinet with each additional axis located 3 meters further. A centralized control system would be characterized by a central control cabinet housing the drives with each motor having separate shielded power and feedback cables adding up to 248 meters of cable.

Instead, a combination of a single KOLLMORGEN AKD-C power supply module and 8 decentralized AKD-N servo controllers would reduce the cable requirement to 34 meters. The calculation: A single 5 meter hybrid cable supplying power and field bus for axis control is connected between the power supply module and the first decentralized controller. A single hybrid cable 3 meters long connects each additional drive for a total of 21 meters. Because we assume that each motor is located 1 meter away from each decentralized AKD-N drive KOLLMORGEN provides a one-cable motor connection technology, only 8 additional meters of cable is required. Overall, the decentralized system reduced the cable requirements from 248 to 34 meters, a savings of 86 percent. These figures represent an idea of the overall monetary gains for the OEM including cable costs and reduction in assembly effort. When the axes require additional I/O the reduction in cabling is even more obvious. Instead of 372 meters, only 42 meters is needed, a corresponding saving of 89 percent.

Another benefit of the relocation of drives is the reduction of power dissipated in the control cabinet. This effectively reduces the requirements for air conditioning thus providing direct saving for both the OEM and end user. As such, the control cabinet air conditioner can be reduced in size or completely eliminated, reducing costs for hardware and subsequent operation – ultimately increasing energy efficiency.

Technical advantages by decreasing complexity

Kollmorgen_Servo Technique_Centralized_Decentralized_KBMThe AKD -N series KOLLMORGEN drives provide IP67 protection and connection via an eleven millimeter diameter hybrid cable to the central supply module in the control cabinet. This single cable provides power and communications without the need for any additional cabling. Each AKD-C supply module can support two strings of AKD -N drives up to 5 kW each, and up to 8 AKD –N drives per string. Safe Torque Off shutdown performed via the hybrid cable comes as standard, and can be implemented for each drive individually or as group. Also, only one cable is necessary between the distributed servo controller and its connected motor thanks to a new single-cable technology. Two cables are no longer required to provide motor power and feedback. In material handling applications where precise motion is demanded, separate cable trays or tow chains are often required for motor and feedback cables. This requirement is now reduced because there is much less cabling.

Winning with increased design freedom

Sample calculations show that the decentralized servo technology saves space in combination with the single-cable connection technology between motor and controller. This benefit results in smaller cable trays, lighter drag chains, and more compactness giving more design freedom in the development of new machines. This freedom resulted primarily from the fact that the distributed technology extends modularization capabilities in comparison to the unflexible, central control design. The bottom line is that this allows new OEM plants to create new machines from already developed modules making the engineering more efficient.

Distributed drive technology as a hybrid

A second way to decentralize is with the use of a hybrid integrated solution. These are combined motor and servo controller units without the need for external wiring. This so-called “piggyback” solution has the disadvantage of drive derating with increased ambient temperature. The higher the ambient the more performance reduction occurs in order for the drive to self-protect from overheating. This relationship ensures in practice that the motors must be larger than otherwise necessary to give the required performance within acceptable temperature limits for the electronics. Typical servo tasks such as rapid acceleration and deceleration during positioning can be especially difficult in the design of hybrid solutions due to the problem of effectively dissipating heat. However, separating the motor and drive at this point prevents the inherent design-related derating. This solution provides the basis for smaller motors in combination with better energy efficiency. In addition, integrated combinations are usually focused on a single motor type, limiting flexibility in the machine design. In contrast, any KOLLMORGEN brushless motor type can be connected to the decentralized AKD-N servo drive. These motors include conventional or direct drive rotary and linear direct drive types, providing true design freedom and optimum performance.

Kollmorgen_Servo Technique_Centralized_Decentralized_OneCableAn integration example

In conclusion, to clarify these relationships an example of servo drive technology for a food processing machine will be shown. The process begins with the cutting of sausage and cheese by a so-called slicer. The product is conveyed onto a belt. The process is not just a simple matter of conveying a sausage stack from point A to B but to transport it as well defined shingles. The need for highly dynamic single axis positioning system is clear. The question now arises how to integrate the required sophisticated motion control functions while maintaining centralized machine control. The slicer provides a good example because it represents a specific decentralized axis because its high power requirement cannot be met with a decentralized drive. The primary objective from the manufacturing perspective is to harmonize highly diverse functional requirements for a wide combination of centralized and decentralized solutions. The KOLLMORGEN AKD-N drive deliberately focuses on the use of a centralized AKD platform. It provides appropriate technology to allow the optimum selection of a motion solution for the performance task required, offered through the wide variety of compatible actuators.
Kollmorgen_Servo Technique_Centralized_Decentralized_Tangel-of-Cables

 

Kollmorgen_Servo Technique_Centralized_Decentralized_Linder

About KOLLMORGEN

KOLLMORGEN is a leading provider of integrated automation and drive systems along with corresponding components for machine builders all over the world. With more than 70 years of Motion Control Design and application experience and profound knowledge of constructing standard and special solutions, KOLLMORGEN supplies solutions time and again that stand out in terms of performance, quality, reliability, and ease of use. As a result customers can achieve a market advantage which is beyond question.
Contact us for more information.

Download as PDF

AKD-N Decentralized Servo Drive

The AKD-N decentralized servo drive reduces cabinet space and opens the way to a smarter machine automation with 80% less cabling. Typical applications for the AKD-N are packaging machines and production machines in food and beverage industry.

  • IP67 drives can be mounted to machine, outside the control panel
  • Reduced cabling because DC, network, power supply, I/O level as well as safety (STO) run in one cable
  • More flexibility in machine design, can be “cold plate” mounted
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Kollmorgen Helps Salvagnini Build More Energy-Efficient Metal-Bending Machines >

Innovation, competency, service. Through 60 years in business, these three commitments have helped the Salvagnini Group achieve global leadership in the field of sheet-metal processing equipment. As the #1 worldwide supplier of panel benders, and one…
Tips and Tricks for the Workbench Scope Tool

Tips and Tricks for the Workbench Scope Tool >

The AKD and AKD2G Scope Tool can be used to capture data in many different ways. These tricks can be used to help you understand the finer points of the tool.
Safe Torque Off (STO) in practice: a Swiss manufacturer of test equipment is already using the TÜV-certified safety technology based on a slip ring and AKD-N servo drives from KOLLMORGEN arranged in a distributed setup.

Kollmorgen and Stemmann-Technik - Safety via Slip Ring >

Safe Torque Off: Kollmorgen and Stemmann-Technik are developing a TÜV-certified solution

Kollmorgen Automation Solutions and Product Catalog EMEA >

Kollmorgen Automation and Motion Control Kollmorgen: Your partner. In Motion. Every solution comes from a real understanding of the challenges facing machine designers and users.
Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…

Kollmorgen AKD-N Servo Drive Brochure EN >

Distributed Servo Technology - The on-site drive for the machine design of tomorrow

MEQuadrat - Rotary Indexing Table - Providing orientation for materials >

Success Story: Swiss company MEquadrat AG builds test systems with decentralized servo technology from KOLLMORGEN.
OMET - Flexographic Printing Machin

OMET - Flexographic Printing Machine - Flexibility and Innovation for Top Printing Quality >

AKD-N decentralized drives and CDDR motors by Kollmorgen are the core of the innovative OMET Xflex X5, a printing solution with the best returns on investment in terms of market result of narrow web printing of labels and flexible packaging.