Europe June 2017  
 
 
  Self-driving systems for internal material flow  
 
     
 
 
 

DC servomotors in KOLLMORGEN’s AKM series with 48 volt winding for autonomous vehicles

 
 
 
 

No name would have been more desirable. With the Packman 200, Opteq Robotics has developed a self-driving solution for material flow which makes its way quickly and directly through the aisles to reach its destination, just like the popular arcade game from the 1980s. While making the wrong turn soon means game over in the classic Japanese arcade game when the main yellow character becomes the victim of voracious ghosts...

 
 
  Read More  
 
 
  Blog in Motion  
 
     
 
 
 

3 Key Reasons for NOT Taking Shortcuts for Motor Repairs

 
 
 
 

Brushless AC servo motors and stepper motors have long life spans, which are largely due to the lack of wearing components. Unlike brush type motors, other than the bearings, brushless AC servo motors and stepper motors have no wearing components...

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
 
  Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
         Request a Quote
 
 
  KOLLMORGEN Europe GmbH, Pempelfurtstraße 1, 40880 Ratingen
Privacy Statement